AXIS#.SAFEPARAM.SBC​.BRAKE#ATTACHED

Description

Indicates whether Safe Brake Control (SBC) is enabled on this axis. Axis 1 can have SBC enabled with two assigned brakes. Axis 2 can only have SBC enabled with one brake (ie: BRAKE2ATTACHED cannot be set).

Value Description

0

No brake configured

1

Brake attached – without SDB (brake is applied before STO occurs according to AXIS#.SAFEPARAM.SBC​.BRAKETIMEDELAY)

2

Brake attached – with SDB (brake is applied after STO occurs)


  • IfAXIS#.MOTOR.BRAKE and BRAKE#.AXIS indicates no brake is attached to the axis but this safety parameter indicates a brake is attached, a warning will occur.

 

Context

For complete SBC information refer to SBC (Safe Brake Control).

Related safety parameters:

Versions

Action

Version

Notes

Implemented

02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0, 1, 2

Default Value

0

Data Type

Integer

Stored in Non Volatile Memory

No